Autonomous security robots
Article
Thermal testing of high-density power components
A key factor in designing high-density power devices is the thermal performance of the internal circuitry. Vicor maximizes efficiency to reduce the losses as far as possible when designing these devices. Even so, the heat generated by residual losses must be dissipated to avoid overheating, which has a direct impact on reliability.
As with the electrical test equipment, much of the all-important thermal testing equipment has been developed by the Vicor R&D department. The sophisticated wind tunnel system is one of the best available on the market, but the specialized thermal measurement equipment, product interfaces, specialized thermocouples and analysis systems are all designed and built in-house.
All test stations, and many non-production ATEs, include sensitive thermal cameras to identify potential hot-spots within the device to ensure the product does not exceed the thermal parameters under all load conditions in order to maximize performance, density and reliability. This detailed thermal analysis, extensive burn-in and the subsequent test data obtained is also used as a direct feed for Vicor comprehensive data sheets.
Vicor considers its high level of investment in design and testing essential to ensure that comprehensive, real-world data are obtained. Investment in development and tools is a top management priority within the company; every operation is equipped to do the job thoroughly. The company’s R&D budget is a high priority and is funded generously as part of the company’s strategy to invest in innovation.
In addition to the accuracy and detail of product datasheets, the investment also means that customers benefit from the many tools and resources available from Vicor. The Vicor suite of tools includes a web-based comprehensive solution selector that enables customers to select the best product for the application together with simulation to show exactly how the product behaves under all conditions. The Whiteboard helps customers configure their own optimized system solution, allowing them to simulate and evaluate performance at a power system level. Test date from real devices is used as the data feed for tools like the Whiteboard ensuring very high accuracy.

Wind tunnel used for thermal testing

Orthogonal thermal conductivity matrix representation of PCB trace and via geometry
コンテンツ
設計エンジニア向けコンテンツ
Autonomous security robots

Tesla commits to 48-Volt automotive electrics
48V is soon to be the new 12V according to Tesla. Size and weight reduction and enhanced power efficiency are a few of the benefits.

BEVs have a weight problem that can’t be solved with traditional approaches
BEVs are getting heavier and adopting a 48V zonal architecture curbs the weight. High-density power modules maximize weight reduction and efficiency.