Kodiak Robotics ushers in a new era of autonomous long-haul transportation.
Powering Innovation: Kodiak Robotics ushers in a new era of autonomous long-haul transportation
Kodiak integrates autonomous technology into commercial trucking fleets powered by Vicor modules

Kodiak Robotics long-haul trucking autonomous technology, the kodiakDriver, includes a modular hardware system, known as SensorPods™, that integrate the majority of sensors needed to “see” its environment using the truck’s traditional mirror-mount points.

Kodiak Robotics long-haul trucking autonomous technology, the kodiakDriver, includes a modular hardware system, known as SensorPods™, that integrate the majority of sensors needed to “see” its environment using the truck’s traditional mirror-mount points.
Commercial trucking is the backbone of the U.S. economy. That has never been more evident than in the past few years, as Covid-19-related supply chain disruptions gripped the country. At the same time, it’s becoming harder and harder to find people who want to drive trucks. The average American truck driver is about 48 years old and for long haul truckers, the average age is even higher, which may help explain why there was a shortage of 80,000 drivers in the U.S. last year, according to the American Trucking Association.
Many industry analysts believe long haul commercial trucking is likely to be the first major use case of autonomous vehicle technology as highway driving is a less complicated problem to solve compared to the many nuances of negotiating secondary roads and city streets.
Additionally, from an economic standpoint, the trucking industry can benefit more from vehicle autonomy. The cost of an autonomous driving system is more easily amortized in a truck that operates for between one million and two million miles. Plus, the average human-driven truck is only used for 7.5 hours a day, due to hours of service limitations. An autonomous truck can double or even triple truck utilization, only stopping to refuel, receive, and pick up new loads.
Kodiak Robotics targets long-haul trucking autonomy
Against that backdrop Kodiak Robotics was launched in 2018 with a focus of developing autonomous technology for the long-haul environment that can be integrated into carriers’ fleets. Kodiak’s autonomous solution, the kodiakDriver, includes a modular hardware system, known as SensorPods™, that integrate the majority of sensors needed to “see” its environment using the truck’s traditional mirror-mount points. The pods’ modular design allows them to be swapped on and off within minutes, which maximizes fleet uptime without the need for specially-trained technicians to install the devices and recalibrate the sensor network.
Kodiak uses a unique Sparse Mapping approach, which contains the information needed to make autonomy possible, rather than data heavy and hard to update HD maps. The maps are complemented by Kodiak Vision, a comprehensive sensor fusion system that utilizes data from radar, cameras and Lidar to see the road in all conditions.
Since launching its operations hub just south of Dallas, Texas, in 2019, Kodiak has been focusing on safely developing a system that can handle the demanding long-haul environment. This year alone Kodiak has completed multiple pilots with some of the biggest names in freight, including four uninterrupted round trips from Dallas to Atlanta with the kodiakDriver continuously operating. Since August 2022, Kodiak has been making autonomous freight deliveries in Texas for home goods retailer IKEA, operating seven days a week between a distribution center in Baytown and the IKEA Store in Frisco.
"The Kodiak team represents some of the most experienced people in the autonomous vehicle industry,” said Don Burnette, the company’s Founder and CEO. “This has allowed us to take the most direct path to success, versus the trial-and-error approach that was common when the industry was starting."
Vicor power solutions exceed demanding and essential sensor qualifications
Kodiak quickly identified three areas in an AV trucking environment where the power system design needs to be uncompromising: reliability, efficiency and the ability to perform in-system health monitoring.
These requirements are what drew Kodiak to partner with Vicor Corporation’s custom design subsidiary, Vicor Power Systems (Vicor). This group designs high-density, high-performance power systems utilizing Vicor’s power modules, that are ideal for autonomous vehicle systems. The Kodiak power system utilizes several Vicor power modules to support their sensor needs that require 12, 24, and 48V power supply buses. These include the Vicor NBM6123, BCM6123, PRMs™ and VTMs™. All of the power modules deliver reliable, highly efficient power conversion in very small packages.
Vicor also provided design support to enable a controllable output feature to every component in the system and optimizing component health by monitoring the voltage and current on all Kodiak sensors. The Kodiak platform includes four basic buses that must be directed to specific sensors, actuators and processors. Each output is monitored and individually controlled through a proprietary CAN bus.
Vicor additionally provides battery charging for a 48-volt system when the truck is garaged and plugged in. The AC shore power system maintains the battery charge level when the engine is not running, allowing maintenance technicians and engineers to use the vehicle indoors. By using a Vicor 48-volt system on the truck Kodiak is able to reduce the size of the cabling, saving weight, space and enabling the vehicle for high-power applications.
Radically changing the future for commercial transportation and truckers
Commercial transportation is underappreciated, yet it is indispensable to global economic stability. Today, Kodiak stands ready to revolutionize this industry with autonomous transportation that will enable more reliable and efficient trucking.
Learn more about Kodiak and how power modules are supporting their next-generation technology.
About Vicor
Vicor Corporation designs, develops, manufactures and markets modular power components and complete power systems based upon a portfolio of patented technologies. Headquartered in Andover, Massachusetts, Vicor sells its products to the power systems market, including enterprise and high performance computing, industrial equipment and automation, telecommunications and network infrastructure, vehicles and transportation, aerospace and defense. www.vicorpower.com
Vicor is a registered trademark of Vicor Corporation.
About Kodiak
The Kodiak Driver is the industry’s most advanced technology stack purpose-built for long-haul trucks, leveraging a unique sensor fusion system and lightweight mapping solution. Today, the Kodiak Driver handles all aspects of highway driving, delivering freight safely, efficiently, and on time.
Founded by a group of self-driving industry veterans intent on helping solve the trucking industry’s greatest challenges, Kodiak is initiating the first widespread adoption of self-driving technology that will save lives, increase network efficiency, reduce costs and emissions, and enhance the quality of life of truck drivers.