Greg Green discusses industry insights on technology innovations for the next gen of EVs
EETimes sponsored a panel discussion on Technology Innovation for the Next Gen of EVs. Learn what Greg Green of Vicor had to say about using power modules
Vicor PI3325 ZVS buck regulators are highly integrated system-in-package regulators that output 5V at up to 20A for point-of-load applications. The PI3325 integrates the controller, power switches, and support components in a 10 x 14mm LGA package and uses a high-performance Zero-Voltage Switching topology to provide best-in-class efficiency, with pulse skipping at light loads. It operates from a 14 to 42 V supply, and supports parallel operation with automatic current sharing for applications with higher current requirements. The PI3325 supports fast and slow current limits, integrates a differential amplifier for remote sensing, and has adjustable soft start and tracking.
Greg Green discusses industry insights on technology innovations for the next gen of EVs
EETimes sponsored a panel discussion on Technology Innovation for the Next Gen of EVs. Learn what Greg Green of Vicor had to say about using power modules
Why choose power modules over discrete power solutions?
There are many advantages of using power modules over home-grown discrete solutions. Learn how power modules can make your next design easier and faster
Lightning Motorcycles accelerates into the EV racing record books
Lightning Motorcycle has built the fastest electric motorcycle on the planet
Vicor engineer Chris Swartz achieves senior member status at Institute of Electrical and Electronics Engineers
Chris Swartz achieves IEEE Senior Member, an elite status held by less than 10% of its members. Swartz has worked at Vicor for 15 years